Improved Shield Design Delivers Higher Voltage Ratings, Up to 20 dB of Radiated E-Field Reduction, and Polarity Marking for Additional EMI Control MALVERN, Pa., June 05, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its IHLE ® series of low profile, high current
WSZ Lead Form Allows Devices to Be Used as SMD Components to Reduce Assembly Costs MALVERN, Pa., May 29, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today announced that 5 W devices in its AC and AC-AT series of cemented, axial-leaded wirewound resistors are now available with
For Automotive Applications, 850 nm and 940 nm Devices Offer High Drive Currents to 1.5 A DC and 5 A Pulsed, Radiant Intensity to 6000 mW/sr in 3.4 mm by 3.4 mm SMD Packages MALVERN, Pa., May 22, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today broadened its optoelectronics
MALVERN, Pa., May 21, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH ), one of the world's largest manufacturers of discrete semiconductors and passive components, announced today that the Company’s Board of Directors declared a dividend of $0.10 per share of common stock and
For Industrial Applications, Device Combines a Low 6 ns Pulse Width Distortion and 2 mA Supply Current With High Temp. Operation to +110 °C MALVERN, Pa., May 15, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 25 MBd high speed optocoupler featuring a CMOS
Featuring a Unique Winding Structure and Building Technique, Customizable Devices Are Qualified to MIL-STD-981 Class S Standard MALVERN, Pa., May 08, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of low profile, space-grade planar transformers for
MALVERN, Pa., May 08, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc., (NYSE: VSH), one of the world's largest manufacturers of discrete semiconductors and passive electronic components, today announced results for the fiscal first quarter ended March 30, 2024.
Fourth-Generation Device Enables Higher Power Ratings and Density Versus D²PAK While Lowering Conduction and Switching Losses to Increase Efficiency MALVERN, Pa., May 01, 2024 (GLOBE NEWSWIRE) -- To provide higher efficiency and power density for telecom, industrial, and computing applications,
Featuring Ferrite Core Technology, Through-Hole Device Offers High Temp. Operation to +155 °C and Low DCR to Reduce Power Losses and Increase Efficiency MALVERN, Pa. , April 24, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new Automotive Grade IHDF
MALVERN, Pa., April 23, 2024 (GLOBE NEWSWIRE) -- Vishay Intertechnology, Inc. (NYSE: VSH) today issued the following statement from its Board of Directors in response to the press release issued on April 22, 2024 by Mountaineer Partners Management, LLC (“Mountaineer”) in which Mountaineer published